The xwr16xx.bin which is stored in SFLAH via FLASH TOOL was like that:
I want to only update the DSS code via QSPI with keeping the BSS and MSS code, so I flash the different dss.bin that I need to update to the position of above picture . But , the bootloader did not load the code successful.
There are CRC in each image , does it cause the error ? if it is , how to calculate the CRC code ? Or there is a better way to change the DSS.bin which is stored in SFLASH ?