This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642BOOST: The Range Resolution settings for Maximum Unambiguous Range of AWR1642BOOST with Demo Visualizer

Guru 16800 points
Part Number: AWR1642BOOST


Hello,

Is there any information for the relationship between "Maximum Unambiguous Range" and "Range Resolution"?
My customers want to achieve the best performance of AWR1642BOOST for the following parameter.
- Range accuracy
- Angle accuracy
- SNR
- Other RF parameters

In my customer's side, they evaluated the following situation.
1. Maximum Unambiguous Range is 25m and Range Resolution is 5cm
1. Maximum Unambiguous Range is 25m and Range Resolution is 10cm

The second one output better results than first.
So, they think that there is the best setting of Range Resolution for Maximum Unambiguous Range with AWR1642BOOST.

Best Regards,

Nomo