This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Guy,
The "xwr16xx_radarss_rprc.bin" is the Radar subsystem firmware file that controls and monitors the RF front end .
This firmware file is used along with the MSS and DSS binary file to create the METAIMAGE that can be flashed to the device.
This would happen during the SDK build process. Below is the screenshot of the METAIMAGE creation during the SDK build:
BR,
Raghu
----------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question.
----------------------------------------------------------------------------------------------------------