Other Parts Discussed in Thread: LDC1612, LDC1101
I have an inductive prox switch where I am currently using an Infineon TC 505 IC. It is a 30 mm switch which I am trying to set a range of 30 mm for. I am using a Bourns 3006 trimpot to dial in my sensing range.
The problem I am having is that some units are experiencing a shift in the sensing range - upwards of 10 mm - from 30mm to 40mm. This increase is causing other problems in the application.
When I get the failed units, i able to 'reset' the switch by readjusting the trim pot but I do not think the trim pot is actually changing.
I am wondering if this 'change' is more a function of the Infineon IC and maybe a different IC may be the answer to my concerns.
I would really like to talk to someone familiar with these Inductive Switch ICs