This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642BOOST: why Ramp end time less than 19 set showing an error?

Part Number: AWR1642BOOST

Hi experts,

My profile cfg file  is described in the table below:

sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 15 3 0
adcCfg 2 1
adcbufCfg 0 0 1 1
profileCfg 0 77 2 2 19 0 0 15.625 1 128 12400 0 0 30
chirpCfg 0 0 0 0 0 0 0 1
frameCfg 0 0 128 1 60 1 0
lowPower 0 0
sensorStart

Q:Why is this blackbody parameter(Ramp end time in u-sec) less than 19  the mmWave_Demo_Visualizer 1.0.0  will showing an error,such as 18 or 12 ect ?

Thanks in advance!

NanShan