This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP75: TMP75 I2C

Part Number: TMP75


Hello Team,

We only define I2C timing requirement for fast and high-speed mode in TMP75 datasheet, Can our part work in standard I2C mode? If yes, what's the timing requirement? Thanks

Regards,

Nanfang

  • Yes, we support Standard Mode as defined in the NXP I2C Spec. Most of this spec is repeated in our datasheet, but formatted in a different way. This is because our device only acts as a Slave, so not all of the parameters are relevant.

    I2C does not have a minimum frequency. Our minimum frequency is indirectly set by our Time-out feature. If you do not complete the I2C Transaction (defined as the time from START to STOP) within 30ms, the device will time-out and reset the interface. This Time-out is a requirement of SMBus that does not exist in the I2C specifcation.

    Ren