Hi all,
We are trying to control a bldc motor using two hall sensors. But before proceeding further i wish to be clear about the calculation behind the hall sensor placement angle (electrical angle).
In three hall sensor configuration why 120/60 angle is most commonly used? What is the calculation behind it. How did we reach at this angle configuration.
We have two hall sensor assemblies available with us(These are two hall sensor configuration i.e only two sensors are placed for control.Third signal is generated using the combination of these two signals). One is with hall sensors placed 90 degrees apart and other with 67 degrees apart. What might be the reason behind this angle? Why not 180 degrees?
Also one thing observed is that with 67 degrees, speed achieved is more. What might be the reason behind that? Is it because the change in states are detected faster in 67 degree configuration?
Regards,
Ann