This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642: Antenna coupling signature and its compensation algorithm in mmw demo

Part Number: AWR1642


Hi champion,
   In AWR1642 mmw demo in mmwave_sdk_01_00_00_05. There is an algorithm switch called calibDcRangeSig. In the user guide there is an explanation 'Antenna coupling signature dominates the range bins close to the rada'.

   Could you elabrate it a bit about what is this antenna coupling and its impact to overall system?  And is there any reference to the algorithm we choose?

Thanks,
Adam

  • Hi Adam

    Antenna coupling is the direct coupling of the Tx antenna signals to the Rx antenna. In the output spectrum it would look like a strong reflector close to DC (or the 0th range bin). A strong antenna coupling signature can 'drown' out the reflected signals from weak reflectors - (for e.g, if you place your hand about 5cm from the device, it may not get detected).

    Antenna coupling would depend on the isolation between the Rx antennas and the Tx antennas. But it would be a stable signature for a given chirp configuration. So we can measure it, and remove it.

    The calibDcRangeSig option simply computes the average chirp (after 1D FFT for a couple of frames) and then subtracts a portion of it from 'every' chirp henceforth. In other words, we estimate the mean signature of the scene and remove it from every measurement afterwards.

    This can help in the case of antenna coupling, because, we know that Antenna coupling is a stable signature, and occurs only very close to the radar. So we use the calibDcRangeSig option to estimate the average chirp, and then remove the stable signature from the first few range bins.

    Regards
    Anil
  • Hi Anil,
       Thanks. It is very helpful:)

    Best regards,
    Adam