This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642: Settings of Advanced Chirp Configurations on AWR1642

Guru 16800 points
Part Number: AWR1642
Other Parts Discussed in Thread: MMWAVE-DFP

Hello,

I have questions for the settings of Advanced Chirp Configurations.
About Figure 8 in swra553, how to set the number of chirp in a burst and the number of burst?
(In the figure, the number of chirp in a burst is 4 and the number of burst is 3.)

I think the number of chirp in a burst can be set by frameCfg.numLoops and the number of burst can be set by chirpCfg.chirpStartIdx and chirpCfg.chirpEndIdx.

Best Regards,

Nomo