This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP421: DXN connected to ground

Part Number: TMP421
Other Parts Discussed in Thread: TMP461

Can the TMP421 be used to temp sense a diode-connected PNP where the anode of the diode is grounded? 

In this application, a power device provides a temp sense pin to monitor the device temperature.  The temp sense pin is configured as a diode-connected pnp, but the anode side of the diode is internally tied to the device ground.  This means with a traditional diode connection to the TMP421, the DXN input would be tied to ground. This pin is internally biased a diode drop above ground.

Will this work?  Or is there another way to connect the diode to the TMP421?