This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642BOOST: running TIDEP-0090 (tmdemo) GUI issue

Part Number: IWR1642BOOST
Other Parts Discussed in Thread: TIDEP-0090, , IWR1642

With IWR1642BOOST, I am testing TIDEP-0090 (tmdemo) reference design.

I compiled and programmed the binary at IWR1642BOOST.

I executed the demo at Windows command prompt as below.

C:\tmdemo\mmwave_demo_dev\radarDemo\chains\RadarReceiverEDMA_mmwSDK\mmw_TMDemo\gui>mmw_demo.exe 24 10 25 mmw_tm_demo.cfg 1
Starting UI for mmWave Demo ....
Opening configuration file mmw_tm_demo.cfg ...

comportnum_str =

COM24


comportnum_str =

COM25

Sending configuration to IWR16xx mmw_tm_demo.cfg ...
dfeDataOutputMode 1
channelCfg 15 3 0
adcCfg 2 1
adcbufCfg 0 1 1 1
profileCfg 0 76 5 0 48 0 0 9.125 1 206 5000 0 0 48
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 2
frameCfg 0 1 46 0 40 1 0
lowPower 0 0
guiMonitor 1 0 0 0
cfarCfg 4 1 18 16 8 4 0 63 0
doaCfg 3 1047 3 600 10 50
dbscanCfg 1 4 12 13 20 3 256
trackingCfg 1 10 10 2 3 25
sensorStart

After executing, there was issue with GUI Window pane.

There is no X-Y Scatter Plot displaying as below.

So, can you check how to solve the issue?

Best regards,

Hayden