This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC7200: a lot of change in TIME2, TIME3 , ...!

Part Number: TDC7200
Other Parts Discussed in Thread: TDC1000

Hello,

i have problem with TDC1000 and TDC7200 for calculate flow!

after a lot of test i found the problem but i couldn't solve it!

my problem is flow have a lot of change! i check all parameters have effect in flow equation, almost all of them are fix in stable flow except one of them! the variable parameter is TIME2!

i checked TIMEs (TIME3,4 and 5) all of them have a lot of change!
you can see in attached file result of one test with this situation:

uint8_t TDC7200_reg_local_copy[10] = {0x02, /*0x58*/0x5C, 0x1F, 0x07, 0xFF, 0xFF, 0xFF, 0xFF, 0x0, 0x0 };
uint8_t TDC1000_reg_local_copy[10] = {0x4F, /*0x59*/0x5D, 0x32, 0x42, 0x1F, 0x80, 0x1F, 0x03, 0x02, 0x00};

10-1-1-RUN-35mv -UP- STOP3-G12 - Result.xlsx

Clock Count TIME1 TIME4 CALIB1 normLSB
702 2152 2131 2322 0.053879
702 2152 2096 2321 0.053892
702 2152 2116 2322 0.053892
702 2152 2069 2322 0.053887
702 2151 1968 2321 0.0539
702 2152 1889 2321 0.0539
702 2152 1903 2321 0.0539
702 2151 1910 2321 0.053897
702 2151 1849 2321 0.0539
702 2151 1882 2321 0.053903
702 2151 1910 2321 0.053897
702 2152 1874 2321 0.053897
702 2151 1888 2321 0.053905
702 2151 1875 2321 0.0539
702 2151 1873 2321 0.05391
702 2151 1862 2321 0.053908
702 2151 1855 2320 0.053915
702 2151 1857 2321 0.053895
702 2151 1880 2321 0.05391
702 2151 1901 2321 0.05391
702 2152 1891 2321 0.053897
702 2151 1902 2321 0.053903
702 2152 1899 2321 0.053895
702 2151 1878 2320 0.053903
702 2152 1881 2322 0.053887
702 2151 1880 2320 0.053915
702 2151 1875 2320 0.053913
702 2151 1905 2321 0.05391
702 2151 1901 2321 0.0539
702 2151 1885 2321 0.053908
702 2151 1879 2321 0.05391
702 2151 1882 2321 0.0539
702 2151 1897 2320 0.05391
702 2151 1917 2320 0.053913
702 2152 1918 2321 0.053892

i checked with different gain , without gain and ...

can you help me how can i fix this parameter?