Dear e2e Community,
My customer needs to define 2 zones:
- zone 1: 0.5-2 meters
- zone 2: 0-0.5 meters
The constraints are wide angle view and solution cost.
1- to lower the cost, can we consider a monostatic topology? what is the minimum blind zone we could expect?
2- as the distance is quite short, should we use a high frequency (also to help on the min detectable range)? or should we work on low freq (to help on the wide angle detection aspect)?
3- can we use direct drive mode in that case?
Regards,