Other Parts Discussed in Thread: LDC2114
Dear Expert,
My customers are evaluating FDC2212.
However, FDC 2212 can not keep the output accuracy required by my customers.
This picture is the actual output characteristic.
The output fluctuates due to the change of the ambient temperature.
Is this normal device-specific condition?
<There are several factors that cause the output to be disturbed>
①Register setting
⇒I reviewed the setting of the register and it seems that it improved a bit.
I will attach a register setting table. Can you check if it is set with wrong register value?
②Circuit design & Design of sensor partial electrode
⇒If you have direct communication, please contact me.
③Temperature characteristic of capacitor
⇒I watched a write like this with another post.
There is no such case, I am in trouble.
I'd like to have a chance to solve problems.
A little advice is OK so please give me a reply.
Best,Regars.
Nor