Part Number: IWR1642
Hi everyone, im trying to use TI demo code to detect power lines (approx 1cm thin) with a max speed of 10 meters/s on a range 15-20 meters.
Can anyone suggest the parameters I should set in demo visualizer?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: IWR1642
Hi everyone, im trying to use TI demo code to detect power lines (approx 1cm thin) with a max speed of 10 meters/s on a range 15-20 meters.
Can anyone suggest the parameters I should set in demo visualizer?
Hello Dmitry,
You should check out the brand new mmWave Sensing Estimator with this link. Here you can configure the mmWave Sensor in a variety of ways and it will automatically show you the desired Chirp Parameters for your specific configuration. I think you're going to find it pretty useful, let me know if you have any questions.
Cheers,
Akash
So, they used the same parameters they used in a chamber experiment? Ok, how then should i set profileCfg parameters for iwr1642?
Another question - how should I set them using SensingEstimator software? I try but sensorr freezes on sensorStart command, or responses with error.
For example:
I set
profileCfg 0 77 7 6.3 59.09 0 0 58.13 1 223 4306 0 0 30
frameCfg 0 1 27 0 33.333 1 0
For this estimator output