Hi,
I have an area of 20x44mm where I have to detect a target at 5mm distance.
The problem I have is when the target is present it will cover 40% of that area but cannot know the position due vibrations. I mean that the target could be anywhere in the area of detection.
In this situation what coil shape do you recommend?
- Racetrack spiral coil. (20x44mm)
- Rectangular coil. (20x44mm)
- 2 Circular coils in series drived by the same LMP91300. (2x 19mm diameter)
- 2 Circular coils drived by different LMP91300. I guess it would be difficult to make them work at different frequencies to avoid interferences between sensors (I have to work below 800KHz). Do you know any rule of thumb about the gap of frequency between sensors to avoid interferences. Also I think itwould be possible to have a "blind" spot between coils.
- Any other suggestion?