Hi champion,
My customer is debuging their own interface board like TI Devpack which is following TI design. Their board can work with Radar studio now, but can't work with TSW1400. They are checking the 120 pin connection on their board. In Devpack's schematics, there are many signals besides the LVDS/CSI2 signals. Could you double check whether all the signals in the schematics are needed?
On customer's board, they connected pin 14,16, [20,22,26,28,32,34,38,40,44,46,50,52,56,58]->CSI2/LVDS, and 93, 94, 96, 106 to the desired signals. Are these signals enough to make TSW1400 work? Plus what is the usage of BP_LP_5V_IN in the connector?
Thanks,
Adam