This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1443BOOST: How to set the number of frames to infinite in Radar studio

Part Number: AWR1443BOOST

Hello,

I want to know how to set the number of frames to infinite in Radar studio.

When I set frameCfg to X X X "0" ......, radar studio said it was invalid setting.

Best Regards

  • Hello Abe-san,

    Setting the "No Of Frames = 0" will set the number of frames to infinite in the RadarStudio.

    -Raghu

    ----------------------------------------------------------------------------------------------------------

    Please click the Verify Answer button on this post if it answers your question.

    ----------------------------------------------------------------------------------------------------------

     

  • Hello Raghu,

    This issue may be related to a limitation when capturing raw data with the TSW1400 board. The Radar Studio manual says the following: To capture raw ADC data in TSW1400, do not enable infinite framing mode (no. of frames = 0) 2. TSW1400 captures frames only for 10 seconds. Hence, ensure that total period of data capture (=frame periodicity x No. of frames) < 10 seconds

    It may be RadarStudio is blocking the infinite number of frames setting as it detected the TSW1400 board.


    Thanks,
    François.
  • Hello Raghu-san, François.-san

    Thanks for your prompt reply.
    If I use combination of AWR and DEVPAK without TSW1400, could I set number of frames to 0 in Radar Studio?

    Best Regards
  • Abe-san,
    From the initial post it was not clear that you are using the TSW1400EVM for data capture and trying to set "Number of Frames :0" .

    Documentation already mentions the limitations wrt to setting infinite framing. You cannot set the number of frames =0 in case of AWR1xx+ TSW1400EVM.

    Thanks,
    Raghu