Other Parts Discussed in Thread: IWR1642
Hello everyone
Based on this thread
I tried all the two methods. However, the board is not running for those two methods. The following is my output from the first method. Can you tell me what the problem is? Thanks.
Xining
C:\ti\mmwave_sdk_01_00_00_05\packages\scripts\windows>generateMetaImage.bat metaImage.bin 0x01000005 C:\Users\xxx\workspace_v7\XXX\16_XXX_mss_v2\Debug\xwr16xx_16_XXX_mss_v2_mss.bin C:\ti\mmwave_sdk_01_00_00_05\firmware\radarss\xwr16xx_radarss_rprc.bin C:\Users\ti\workspace_v7\XXX\16_MMW_dss\Debug\xwr16xx_mmw_demo_dss.bin
c:/ti/mmwave_sdk_01_00_00_05/packages\scripts\ImageCreator\xwr16xx\multicore_image_generator\MulticoreImageGen.exe LE 37 0x01000005 metaImage.bin 0xb5510000 C:\ti\mmwave_sdk_01_00_00_05\firmware\radarss\xwr16xx_radarss_rprc.bin
Number of Input Files 1
Number of zeros 8
call c:/ti/mmwave_sdk_01_00_00_05/packages\scripts\ImageCreator\xwr16xx\crc_multicore_image\crc_multicore_image.exe metaImage.bin metaImage.bin.tmp
size of App Image is 136256 bytes
cur_crc_read_addr 64
Failed to remove CRC temp file
perl c:/ti/mmwave_sdk_01_00_00_05/packages\scripts\ImageCreator\xwr16xx\append_bin_crc\gen_bincrc32.pl metaImage.bin
>>>> Binary CRC32 = aa5984aa <<<<
>>>> Total bytes in binary file 136260 <<<<
C:\ti\mmwave_sdk_01_00_00_05\packages\scripts\windows>