Other Parts Discussed in Thread: IWR1443
Hello,
In page 9 of SWRA554.pdf, it introduces how to configure a device in MIMO mode, but I still confused about configuring MIMO in Radar Studio.
For IWR1443+DevPack+TSW1400, how can I set 2 Tx working alternately?
In Radar Studio->SensorConfig->Chirp tag, it has 'Start Chirp for Cfg' and 'End Chirp for Cfg', and in Frame tag, it has 'Start Chirp TX' and 'End Chirp TX'.
If I want to set 2 Tx working alternately, I need to set 'Start Chirp for Cfg'=0, 'End Chirp for Cfg'=0, and TX Enable for current chirp = TX1; then, 'Start Chirp for Cfg'=1, 'End Chirp for Cfg'=1, and TX Enable for current chirp = TX2. Then in Frame tag, I need to set 'Start Chirp TX'=0 and 'End Chirp TX'=1, which means in one frame, chirp with TX1 and chirp with TX2 work alternately.
Q1: Is my setting correct?
Q2: In Chirp tag, if I set 'Start Chirp for Cfg'=0, 'End Chirp for Cfg'=1, or 'End Chirp for Cfg' bigger than 0 (say 100), is this setting legal, and what does this setting mean?