Other Parts Discussed in Thread: TDC1000, TDC7200
Respected sir,
I want to test Accuracy TDC1000-TDC7200EVM for flow meter application for this requirement I have studied about the TDC-1000 (AFE ) and TDC-7200(Stop watch Timer) Data sheets.
While studying this TDC-1000 (AFE ) and TDC-7200(Stop watch Timer) Data sheets, I got a some doughts Please clarify my Doughts regarding this Topic.
TDC-1000 (AFE ):
1.what happened if number of transmitted pulses are increased from 5 to 10 pulses ?
2.what happened if number of Stop pulses are increased from 2 to 5 pulses?
3.what happened if Threshold voltage (ECHO_QUAL_THLD) is changed from minimum to maximum ?
4.what happened if the LNA is enabled and LNA is disabled ?
5.what happened if the PGA gain is enabled and PGA gain is disabled ?
6.what happened if the Damping is enabled and Damping is disabled?
7.what happened if transmitting pulse position shifting (TX_PH_SHIFT_POS) is changed from minimum to maximum ?
8.When Short TOF measurement is used And Standard TOF measurement is Used ?
9 what happened if the sensor interfacing circuit is not used between the ultrasonic sensor and TDC-1000 (AFE ) ?
TDC-7200(Stop watch Timer):
1.what happened if the calibration value is changed from 10 to 40 clock cycles ?
2.What happened if the force calibration is not happened per every measurement (Difference between Calibration is not performed after interrupted measurement and Calibration is always performed at the end )?
Please Give Reply As soon as possible.
Thanking you sir.
Regards,
K.manikanta.