This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

mmWave TI Resource Explorer Update : mmWave Training v:1.3.0

All,

mmWave content on TI Resource Explorer  is updated with mmWave Training v:1.3.0 which includes Experiments and Chirp configurations as below:

 

Experiments demonstrate the usage of TI mmWave sensors in common use cases such as detecting objects of certain sizes at various distances, detecting walls made up of different materials and detecting height of objects/people passing through a Garage door etc.  Each experiment includes description, set up, methodology, test results and conclusion along-with both physical and software setup information, so the customer can easily replicate the results . Advance algorithms and signal processing may provide even better performance than highlighted in these experiments

 

Chirp database presents users with options for various mmWave RF-Front End chirp configurations which have been implemented for very specific use cases and/or End Equipment. The database is sortable on various fields such as Target device, Range, Velocity, Range Resolution etc. and the selected configuration can be loaded directly into mmWave Sensing Estimator.

 

Both these features can be accessed through TI Resource explorer either in CCS or on the web at http://dev.ti.com/tirex/#/?link=Software%2FmmWave%20Training.

 

Please continue to use mmWave Sensors Forum.

mmWave Team