Other Parts Discussed in Thread: AWR1243
Hello,
I am working with the BOOST board at the moment, and I am also considering the design of a custom breakout board for the IWR1642 IC. So I am wondering about any limiting parameters and properties on the antenna design.
I have read in another post that impedance matching of 50Ohms is optimal. Is this for a single antenna trace? Of for each set of TX and RX antennae?
Given this impedance limit, can you recommend any tips about antenna shape. For example, what was the reason behind designing the antennae having square nodes on the BOOST board. Does larger surface area increase gain? And how to determine optimal antenna shape?
Lastly, I was wondering if you can see any issue with having the antenna lines to be insulated wires of about 40cm. If the impedance can be matched to 50Ohms, then what other factors in such a long wire can affect signal gain? Maybe you guys already have experience in testing longer antennas. Will EMI be significant?
Thank you