Hi,
I am using AWR1243BOOST for long range application. I am trying to find out ways to extend the max range that I can detect in my system.
Using mmWave Sensing Estimator, I see that by increasing the tranmit power and tx and Rx gain, I am able to increase the Max range for typical detectable object. I also understand the concept and formula behind these calculation.
What I would like to know is :
1. What is the Max value of the Transmit power, Tx gain and Rx gain that I can use with the EVM. I am not considering any hardware changes to EVM. I also would like to know that, if there are any other restrictions on these parameters.
2. The values for additional parameters like detection loss, system loss, implementation margin and detection SNR play a role in my calculation here. I would like to know the concept behind the values assumed by mmWave sensing estimator.
2a)An added doubt is, If my EVM is being covered by a thin metal sheet, should I increase the detection loss or system loss factor??
Thanks & Regards,
Santhana Raj