Other Parts Discussed in Thread: AWR1642, AWR1243, AWR1443
Hello there
I want to start the Tx2 at the time that Tx1 is in its half way of operating. For example the chirp length is 20us. Tx1 starts at 0us, and Tx2 starts at 10us.
Based on my understanding of mmWave chip, I can divide the 2 chirps into 4 chirps, as showing below. However, by doing so, in the transmitter side, I need to set the 2Tx with two different chirp configuration and start to transmit at the same time. In the receiver side, I need to switch the reference signal from one to another. Do you think it is doable? Beside this method, can I just set configuration for 2 chirps and start the Tx1 and Tx2 with half chirp length delay?
Thanks
Xining