1-We are trying to apply a BPM MIMO code however the radarstudio GUI is confusing
Our understanding is that all Transmitters are ON and we need only one bit to set the phase to 0 or 180 but there are two bits here which are called TX off and TX on.
What are TXoff and TXon bits and how do you set them for phase 0 or 180 for example for TX1 ?
Explanation in radarstudio manual is very basic and does not answer this question.
Please provide an example
2-After these settings are done what are the follow up steps we need to follow for BPM MIMO? how do we make sure the radar is not TDM MIMO anymore and working in BPM mode.
Thanks