This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1243BOOST: Radar Studio error when using TSW1400 EVM to capture ADC data.

Part Number: AWR1243BOOST
Other Parts Discussed in Thread: AWR1243

Hello,

       I want to use AWR1243EVM+Devpack+TSW1400EVM to capture raw ADC data. And I just follow the approach from

https://training.ti.com/mmwave-sensor-raw-data-capture-using-tsw1400-board?cu=1128486 . After I selected the values in the Config tab of Radar Studio and clicked the  button:SetUp TSW1400, TSW1400 ARM, the Radar Studio output windows showed the following error :

GM: Constructor
GM: Wed Oct 11 21:30:45 2017
RSTD.Transmit("/Settings")
[21:30:45] 
[21:30:45]  ### Running Startup script: "F:\software\TI_DFP\rf_eval\radarstudio\Scripts\Startup.lua" ###
[21:30:45]  RSTD.SetAndTransmit ("/Settings/Scripter/Display DateTime" , "1")
[21:30:45]  RSTD.SetAndTransmit ("/Settings/Scripter/DateTime Format" , "HH:mm:ss")
[21:30:45]  Scripter ignored: Attempt to UnBuild() again or before Build.
[21:30:45]  RSTD.SetVar ("/Settings/Clients/Client 0/Dll" , "F:\\software\\TI_DFP\\rf_eval\\radarstudio\\Clients\\\\LabClient.dll")
[21:30:45]  RSTD.SetVar ("/Settings/Clients/Client 0/Use" , "TRUE")
[21:30:45]  RSTD.SetVar ("/Settings/Clients/Client 1/Use" , "FALSE")
[21:30:45]  RSTD.SetVar ("/Settings/Clients/Client 2/Use" , "FALSE")
[21:30:45]  RSTD.SetVar ("/Settings/Clients/Client 3/Use" , "FALSE")
[21:30:45]  RSTD.SetVar ("/Settings/Clients/Client 4/Use" , "FALSE")
[21:30:45]  RSTD.SetVar ("/Settings/AL Client/AL Dll" , "F:\\software\\TI_DFP\\rf_eval\\radarstudio\\RunTime\\SAL.dll")
[21:30:45]  RSTD.SetVar ("/Settings/Clients/Client 0/GuiDll" , "")
[21:30:45]  RSTD.SetVar ("/Settings/AutoUpdate/Enabled" , "TRUE")
[21:30:45]  RSTD.SetVar ("/Settings/AutoUpdate/Interval" , "1")
[21:30:45]  RSTD.SetVar ("/Settings/Monitors/UpdateDisplay" , "TRUE")
[21:30:45]  RSTD.SetVar ("/Settings/Monitors/OneClickStart" , "TRUE")
[21:30:45]  RSTD.SetVar ("/Settings/Automation/Automation Mode" , "false")
[21:30:45]  RSTD.Transmit("/")
[21:30:45]  RSTD.SaveSettings(): Settings saved to "C:\Users\DELL\AppData\Roaming\RSTD\config.xml"
[21:30:45]  RSTD.Build()
[21:30:45]  RSTD.SaveSettings(): Settings saved to "C:\Users\DELL\AppData\Roaming\RSTD\config.xml"
[21:30:45]  RSTD.Transmit("/")
[21:30:45]  RSTD.AL_Build()
[21:30:45]  RSTD.AL_LoadXml()
[21:30:45]  RSTD.Transmit("/")
[21:30:45]  RSTD.AL_Init()
[21:30:45]  RSTD.Clients_Build()
[21:30:45]  GM: Init
[21:30:45]  GM: Loaded 'F:\software\TI_DFP\rf_eval\radarstudio\Clients\\LabClient.dll'
[21:30:45]  GM: 1 Guest (s) init
[21:30:45]  GM: 1 Module(s) init
[21:30:45]  GM: 2 Tab   (s) init
[21:30:46]  RSTD.Client_LoadXml()
[21:30:46]  [RadarAPI]: Starting Matlab Engine..
[21:32:33]  [RadarAPI]: Matlab Engine Started!
[21:32:42]  [RadarAPI]: ar1.LoadSettings('C:\Users\DELL\AppData\Roaming\RSTD\ar1gui.ini')
[21:32:44]  TESTING = false
[21:32:44] 
[21:32:44]  ***Script completed successfully.***
[21:33:09]  [RadarAPI]: Opening Gpio Control Port()
[21:33:09]  [RadarAPI]: Status: Passed
[21:33:09]  [RadarAPI]: Opening Board Control Port()
[21:33:09]  [RadarAPI]: Status: Passed
[21:33:10]  [RadarAPI]: ar1.FullReset()
[21:33:10]  [RadarAPI]: Status: Passed
[21:33:11]  [RadarAPI]: Closing Board Control Port()
[21:33:11]  [RadarAPI]: Status: Passed
[21:33:11]  [RadarAPI]: Closing Gpio Control Port()
[21:33:11]  [RadarAPI]: Status: Passed
[21:33:11]  [RadarAPI]: ar1.SOPControl(2)
[21:33:11]  [RadarAPI]: Status: Passed
[21:33:13]  [RadarAPI]: ar1.Connect(6,921600,1000)
[21:33:17]  [RadarAPI]: Warning: Connected with baudrate 115200
[21:33:18]  [RadarAPI]: Warning: Disconnected existing BaudRate
[21:33:18]  [RadarAPI]: Warning: Trying to connect with baudrate 921600
[21:33:20]  [RadarAPI]: ar1.Calling_IsConnected()
[21:33:20]  [RadarAPI]: ar1.SelectChipVersion("XWR1243")
[21:33:20]  [RadarAPI]: Status: Passed
[21:33:21]  [RadarAPI]: ar1.SelectChipVersion("XWR1243")
[21:33:21]  [RadarAPI]: Status: Passed
[21:33:21]  [RadarAPI]: ar1.SaveSettings('C:\Users\DELL\AppData\Roaming\RSTD\ar1gui.ini')
[21:33:39]  [RadarAPI]: ar1.DownloadBSSFw("F:\\software\\TI_DFP\\firmware\\radarss\\xwr12xx_xwr14xx_radarss.bin")
[21:33:40]  [RadarAPI]: Downloading BSS ROM Legacy Binary..
[21:33:50]  [RadarAPI]: ar1.DownloadMSSFw("F:\\software\\TI_DFP\\firmware\\masterss\\xwr12xx_masterss.bin")
[21:33:51]  [RadarAPI]: Downloading MSS Legacy Binary..
[21:34:09]  [RadarAPI]: ar1.PowerOn(0, 1000, 0, 0)
[21:34:09]  [RadarAPI]: Status: Failed, Error Type: RESP TIMEOUT
[21:34:09]  [RadarAPI]: ar1.SaveSettings('C:\Users\DELL\AppData\Roaming\RSTD\ar1gui.ini')
[21:36:01]  [RadarAPI]: ar1.RfEnable()
[21:36:01]  [RadarAPI]: Status: Failed, Error Type: INVALID INPUT
[21:36:01]  [RadarAPI]: Error Occurred in Port open close
[21:36:13]  [RadarAPI]: ar1.PowerOn(0, 1000, 0, 0)
[21:36:13]  [RadarAPI]: Status: Passed
[21:36:13]  [RadarAPI]: ar1.SaveSettings('C:\Users\DELL\AppData\Roaming\RSTD\ar1gui.ini')
[21:36:13]  [RadarAPI]: Unknown Async event recieved(0)
[21:36:20]  [RadarAPI]: ar1.RfEnable()
[21:36:20]  [RadarAPI]: Status: Failed, Error Type: RESP TIMEOUT
[21:36:20]  [RadarAPI]: Warning: Mismatched MSS firmware version!
[21:36:21]  [RadarAPI]: Warning: BSS firmware version Mismatch!
[21:37:00]  [RadarAPI]: ar1.ChanNAdcConfig(1, 0, 0, 1, 0, 0, 0, 2, 2, 0)
[21:37:01]  [RadarAPI]: Status: Failed, Error Type: RESP TIMEOUT
[21:37:05]  [RadarAPI]: ar1.LPModConfig(0, 0)
[21:37:06]  [RadarAPI]: Status: Failed, Error Type: RESP TIMEOUT
[21:37:08]  [RadarAPI]: ar1.RfInit()
[21:37:09]  [RadarAPI]: Status: Failed, Error Type: RESP TIMEOUT
[21:37:14]  [RadarAPI]: ar1.DataPathConfig(1, 1, 0)
[21:37:15]  [RadarAPI]: Status: Failed, Error Type: RESP TIMEOUT
[21:37:56]  [RadarAPI]: ar1.LvdsClkConfig(1, 1)
[21:37:57]  [RadarAPI]: Status: Failed, Error Type: RESP TIMEOUT
[21:38:00]  [RadarAPI]: ar1.LvdsClkConfig(1, 1)
[21:38:01]  [RadarAPI]: Status: Failed, Error Type: RESP TIMEOUT
[21:38:04]  [RadarAPI]: ar1.LVDSLaneConfig(0, 1, 0, 0, 0, 1, 0, 0)
[21:38:05]  [RadarAPI]: Status: Failed, Error Type: RESP TIMEOUT
[21:38:20]  [RadarAPI]: ar1.ProfileConfig(0, 77, 100, 6, 60, 0, 0, 0, 0, 0, 0, 29.982, 0, 256, 10000, 0, 0, 30)
[21:38:21]  [RadarAPI]: Status: Failed, Error Type: RESP TIMEOUT
[21:38:34]  [RadarAPI]: ar1.ChirpConfig(0, 0, 0, 0, 0, 0, 0, 1, 0, 0)
[21:38:35]  [RadarAPI]: Status: Failed, Error Type: RESP TIMEOUT
[21:38:48]  [RadarAPI]: ar1.DisableTestSource(0)
[21:38:49]  [RadarAPI]: Status: Failed, Error Type: RESP TIMEOUT
[21:38:49]  [RadarAPI]: ar1.FrameConfig(0, 0, 32, 128, 40, 0, 1)
[21:38:50]  [RadarAPI]: Status: Failed, Error Type: RESP TIMEOUT
[21:38:50]  [RadarAPI]: MatlabProc Status: Failed
[21:41:31]  [RadarAPI]: ar1.SetupTSW1400()
[21:41:42]  [RadarAPI]: TSW1400 set-up complete.
[21:42:34]  [RadarAPI]: ar1.StartTsw1400Arm("F:\\adc_data.bin")
[21:42:36]  [RadarAPI]: Error:
[21:42:36] 
[21:42:36]  ... MWMCR::EvaluateFunction error ...
[21:42:36]  11-Oct-2017 21:42:34: Frame Config has not been populated,1,
[21:42:36]  Error in => setup_for_triggered_capture_max_30_frames.m at line 6.
[21:42:36] 
[21:42:36]  ... Matlab M-code Stack Trace ...
[21:42:36]      at
[21:42:36]     file C:\Users\DELL\AppData\Local\Temp\DELL\mcrCache8.5.1\Matlab0\Logging\log_status.m, name log_status, line 32.
[21:42:36]      at
[21:42:36] file C:\Users\DELL\AppData\Local\Temp\DELL\mcrCache8.5.1\Matlab0\MatlabPostPr\setup_for_triggered_capture_max_30_frames.m, name setup_for_triggered_capture_max_30_frames, line 6.
[21:42:36] 
[21:42:36] 
[21:42:36]  Trace:
[21:42:36]     在 MathWorks.MATLAB.NET.Utility.MWMCR.EvaluateFunction(String functionName, Int32 numArgsOut, Int32 numArgsIn, MWArray[] argsIn)
[21:42:36]     在 MathWorks.MATLAB.NET.Utility.MWMCR.EvaluateFunction(String functionName, MWArray[] argsIn)
[21:42:36]     在 MatlabPostProcGui.MatlabPostProcGUIClass.setup_for_triggered_capture_max_30_frames(MWArray FilePathWithName)
[21:42:36]     在 AR1xController.frmAR1Main.iStartTSW1400IF()

 
       I have installed the Matlab runtime v8.5.1 win32 bit , and my computer install the Matlab 2014b. If the Matlab runtime v8.5.1 win32 bit conflicts with existing Matlab 2014b.

 Can anyone help me? thanks a lot !

-Jason

conflict with an existing Matlab installtion

  • Jason,
    This is not the issue with Matlab runtime engine.
    I see that your SPI connect and RF powerup are not successful.

    [21:34:09] [RadarAPI]: ar1.PowerOn(0, 1000, 0, 0)
    [21:34:09] [RadarAPI]: Status: Failed, Error Type: RESP TIMEOUT
    [21:34:09] [RadarAPI]: ar1.SaveSettings('C:\Users\DELL\AppData\Roaming\RSTD\ar1gui.ini')
    [21:36:01] [RadarAPI]: ar1.RfEnable()
    [21:36:01] [RadarAPI]: Status: Failed, Error Type: INVALID INPUT

    Can you send the snapshot of the RadarStudio after loading the firmware ?

    -Raghu
  • -Raghu
         Thanks for your reply. Here is the snapshot of the RadarStudio after loading the firmware:
    snapshot_1

    When i kicked the buttun"SPI Connect", the SPI Connectivity Status is still red. then i kicked "RF Power-up",the output window showed:
    [20:54:41]  [RadarAPI]: ar1.PowerOn(0, 1000, 0, 0)
    [20:54:41]  [RadarAPI]: Status: Failed, Error Type: RESP TIMEOUT
    [20:54:41]  [RadarAPI]: ar1.SaveSettings('C:\Users\DELL\AppData\Roaming\RSTD\ar1gui.ini')
    [20:56:50]  [RadarAPI]: ar1.RfEnable()
    [20:56:50]  [RadarAPI]: Status: Failed, Error Type: INVALID INPUT
    [20:56:50]  [RadarAPI]: Error Occurred in Port open close
    And i kicked "SPI Connect" again, SPI is connected.

    then I kicked "RF Power-up" again, the bss/mss firmware version is missing. just like this:

    snapshot_2

    and the output window showed:
    [20:57:31]  [RadarAPI]: ar1.PowerOn(0, 1000, 0, 0)
    [20:57:31]  [RadarAPI]: Status: Passed
    [20:57:31]  [RadarAPI]: Unknown Async event recieved(0)
    [20:57:31]  [RadarAPI]: ar1.SaveSettings('C:\Users\DELL\AppData\Roaming\RSTD\ar1gui.ini')
    [20:58:27]  [RadarAPI]: ar1.RfEnable()
    [20:58:27]  [RadarAPI]: Status: Failed, Error Type: RESP TIMEOUT
    [20:58:28]  [RadarAPI]: Warning: Mismatched MSS firmware version!
    [20:58:28]  [RadarAPI]: Warning: BSS firmware version Mismatch!
           Now  i konw the RF Power-up is failed, but i still don't how to solve it. And i guess that the power supply for AWR1243EVM is wrong. I use 5V/1A power supply  rather than 5V/>2.5A becase there is no enough power supplying 5V/>2.5A. maybe the power supply caused the fail of RF enable. and i will change the power supply as soon as possible.
          Thanks,
    -Jason

  • -Raghu


            I'm sorry for that the snapshots can't upload. I have tried many times but it can't work. the first snapshot is after loading the firmware, the BSS firmware version: 1.7.0.4(19/04/17) ; the MSS firmware version: 1.7.0.0(31/03/17) ; The second snapshot is after kicking the "RF Power-up"again, the bss/mss firmware version :0.0.0.0(00/00/00).


           Sorry for that!


    -Jason

  • -Raghu

            I have changed power supply for AWR1243 EVM ,but it doesn't work , the same error occured. the RF Enable failed .

           I don't know where is wrong? Can you help me?

    -Jason 

  • Hello Jason,

    Which firmware are you using?

    Please be sure to use the firmware found at C:\ti\mmwave_dfp_00_07_00_04\rf_eval\rf_eval_firmware.

    Regards,

    Adrian