This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642: Memory Requirement based on Range FFT=1024, Doppler FFT=64, TDM-MIMO 2T4R

Part Number: AWR1642


Hi,

It looks AWR1642 is not able to achieve the following spec:

Range FFT = 1024  (Samples per chirp)

Doppler FFT = 64 (Chirp per frame)

2T and 4R for TDM-MIMO BPM

FFT processing is 16 bits

The application is SRR

It needs at least 1024*64*4*2*2 bytes (~1M bytes) in L3 memory.

Is my understanding correct? 

If AWR1642 is not enough for this kind of spec. Will enhanced part number has enough L3 memory? (768K+512K??)