Other Parts Discussed in Thread: OPT3001
Hello,
We are thinking of using the OPT3002 sensor to monitor the optical power to which the sensor is being exposed to. For this monitoring system we are interested in the discrimination of the optical power per wavelength. My question is, how can we do this with the OPT3002?
Should I just use the equation 4 present on chapter "Compensation for spectral response" (Optical_Power at Wavelength W = Optical_Power at 505 nm / R)? For example, if the sensor is being exposed to daylight, and I want to know the optical power at wavelength 400nm, 500nm and 600nm, should I just take the value reported by OPT3002 and decompose it on this 3 wavelengths using equation 4 present on chapter "Compensation for spectral response"?
Regards,
Carlos