Other Parts Discussed in Thread: IWR1443, AWR1243
Hi everyone:
Currently we're developing a product end expecting the mmwave radar to sense its surroundings and build a 3D map for further obstacle avoiding and navigation tasks.
Here are some questions about it: (The development board I'm using is the IWR1443 BOOST)
1. Is IWR1443 able to do 3D imaging, i.e., get a 3D scanning of the surrounding environment, for example, get distance value along every direction across azimuth and elevation? In the MmwDemo, the angle estimation is based on detected object since I think it’s not an imaging task.
2. If 3D imaging is possible, is the MmwDemo be able to be altered to do this task? In the Demo, the angle FFT and angle estimation seemed to be based on object detection (CFAR) results.
3. In demo visualizer tool, is there any tool for displaying 3D results, such as detected object in 3D coordinate system, and of course it's even better if 3D imaging results are available?
4. In the Demo visualizer, there is a plot named as “Range-Azimuth Heat Map”, is this a 2D imaging plot?
Thanks very much:)
[unlocked 1/19/18]>LE