Other Parts Discussed in Thread: IWR1443
Hello,
I would like design presence sensor with mmWave IWR1443 on the a steel silo.
the sensor is planning to mounted out of the silo to detect grain presence into silo. (The steel silo thickness is 4mm)
Q1: Can I apply mmWave as presence sensor out of the metal silo to detect grain into silo?
Q2: Could the signal effected metal silo thickness? (I just confuse that can the signal detect meterial/things behind the 4mm metal thickness?)
All the best,
Mehmet
@:mehmettaspinar@endustriyel.com
[unlocked 1/24/18]>LE