This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT8241-CDK-EVM: questions about laser(led) driver in opt8241

Part Number: OPT8241-CDK-EVM

hello

We are going to try test laser module in opt8241 illumination board.

So i modified your reference circuit both QUAD_LASER and HEX LASER like below circuit.

I am wondering several things about below circuits.

1. QUAD_LASER  driver

1) I think anode voltage (net : illum_quad_laser) is 5V . that is not enough to operate laser . Because  Sum of foword voltage is over 9V. I guess.

2) What is SN74LVC2T45 u13 purpose? only to increase amplitude of TRIG ?. IF TRIG high volage is 5v, we can remove u13?

3) IF i design circuit like this . does it work correctly until 3A (Laser peak current) ?  TRIG :  freq = 12MHz / duty : 50%   

   if we should modify else, could you plz some advice?

2. HEX LED DRIVER

1. How much voltage ILLUM_HEX_LED ? ( Boost circuit 's out voltage)   How about  peak current of led?

2. Why annode(D7) needs voltage (ILLUM_HEX_LED)?

3. IF i design circuit like this . does it work correctly until 3A (Laser peak current) ?  TRIG :  freq = 12MHz / duty : 50%   

  if we should modify else, could you plz some advice?

best  regards.