Hello,
If I have pair of AWR1243BOOST + MMWAVEDEVPACK boards, can I configure them in master/slave architecture ?
Are there provisions to take the sync out and send it to sync in of other boost board, fmcw_clkout and 40 MHz crystal clock ?
If this is possible, then is the firmware capable of setting up the devices in multichip master/slave configuration ?
Thank you,
RJ