This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDC1101: LDC1101 Reference input Frequency (Max Value)

Part Number: LDC1101

Hello,

Customer is designing LDC 1101.
The maximum value of Reference Input Frequency of LDC 1101 is 16 MHz.
When using an external oscillator (16 MHz), how many ppm can it be used?
The customer estimates to about ± 50 ppm (16.08 MHz).

Best Regards,
sopatopa