This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE4490SPO2EVM: Operating just one LED?

Part Number: AFE4490SPO2EVM
Other Parts Discussed in Thread: AFE4490

I'd like to operate just one LED and I've configured the EVM to do so as shown in the screenshot. But this means that 50% of the cycle is wasted. I'm not able to change the duty cycle to be higher than 25%, can this be achieved in the AFE4490?