Hi,
I've a HDC1010 sensor on a PCB mounted as per the guidelines in the datasheet. Additionally, I've placed a small 0.9mm circular hole in the under side of the PCB , under the sensor to allow for free air circulation to the sensor. The humidity is somewhat fixed at ~37% while the actual reading from a calibrator is 55%. It doesn't alter much either when a burst of mist is directed at the sensor top or through the circular hole on the bottom side. The Temperature sensor on the same DUT is quite accurate though.
Could someone advise any resolution steps if faced with this issue earlier.
Thanks
Sudhansu Mishra