Other Parts Discussed in Thread: AWR1443, , AWR1642
Hi,
I am working in a project to develop long rang ( 200 m) radar speed display
I need to know what is the suitable EVM (awr 1243or AWR1443 or AWR1643) for this application
Thank you,
Karim
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Karim,
The AWR1243 is intended to output raw ADC samples which is then post processed by external host/ data capture (TSW1400EVM) .AWR1243 is closed front end device and all the configurations happen via the API commands to the front end over SPI interface.
The AWR1443 has the hardware accelerators that do the processing of the ADC data .
The AWR1642 has the integrated DSP for data processing.
Below is the link for the TI mmwave-sensing products and the comparison of the 3 devices.
Looking at your target application AWR1642 seems best fit.
Thanks,
Raghu
Hi Anil ,
Thank you for your Answer,
I would like to use the antenna incorporated with EVM awr1643 ,
Is this antenna just for the short range or can I use it for medium and long range ?
Thank you for your help
Karim