Other Parts Discussed in Thread: UNIFLASH, AWR1243
Hi,
I am trying to run awr1243boost in functional mode(SOP4) in RADAR_STUDIO , as per description it should show correct version of firmware for bss and mss after flashing (SOP5) and, but it is not flashing the provided binaries in dfp-sdk using radar studio in flash mode also it is not enabling RF power up and throwing error
ar1.RfEnable()
[14:31:55] [RadarAPI]: Status: Failed, Error Type: RESP TIMEOUT,
so I tried flashing with uniflash, it is has flashed successfully .
Now if i check on radar studio to run in functional mode still it is not enabling RF power up , it is showing correct firmware version for BSS but not showing for MSS, ultimately what i think is to run in functional mode there should be correct firmware present , i am giving correct firmware but still it is not powering up RF, so I can not configure further with settings.
please help.