This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TDC1000-TDC7200EVM: TDC1000-TDC7200EVM: low power mode and Firmware Build error in CCS

Part Number: TDC1000-TDC7200EVM

Tool/software: Code Composer Studio

Hello,

I am using TDC1000-TDC7200EVM with MSP430F5528 MCU and I have two questions about it.

1) I would like to evaluate the power consumption in low power mode of the TDC1000-TDC7200EVM board wiht differents configurations.

But the firmware on the MSP430F5528 does not have a low power mode and would like to know if you a firmware with low power mode such as the firmware of this eval board : http://www.ti.com/tool/TIDM-ULTRASONIC-FLOW-TDC ?

2) My second question is, I have the same problem with this post :
https://e2e.ti.com/support/sensor/ultrasonic/f/991/p/577894/2121524?tisearch=e2e-sitesearch&keymatch=CCS%2FTDC1000-TDC7200EVM%3A%20Firmware%20Build%20error%20in%20CCS#2121524

I imported the files from C:\Program Files (x86)\Texas Instruments\TDC1000_7200EVM\Firmware\TDC1000_7200EVM_Firmware_Source-v2.01 using Import Project in CCS but when I bluild this project I get the same errors:

My CSS version is 7.3 and I have a WIndows 7.

Any suggestions on how to solve this issue?

Best regards

Kistler Mickaël

  • Hello,

    1. Currently the only firmware available is that which is already included with the TDC1000-TDC7200EVM. The firmware used in that TI design is available for download on that page for reference, but some of the power saving measures available for that particular MSP430 device may not be possible withe the MSP4305528. You may be able to get a better response with some suggestions on maximizing the power savings by creating a post about the MSP4305528 and posting in the MSP430 forum here: e2e.ti.com/.../

    2. I will have to get back to you on this. Currently I am seeing a similar issue.