This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642BOOST: AWR1642BOOST

Part Number: AWR1642BOOST
Other Parts Discussed in Thread: MMWAVE-SDK

Hello,

I download the  mmwave_sdk_01_01_00_02 package (for Windows) from TI website to install the drivers to use the AWR1642Boost.

Basically what I did is :

1 ) power up both PCB AWR1xxBooster and mmWaveDevpack using the 5V power supply and micro usb ( till know I have an open discussion with TI why the mmWavePack is not fullfill powered up since the led S7 is not glow)

2) Go to the device manager in windows what I see is :

Right click on both XDS110  to install the driver. To do that I went to the foldr FTDI but all times I got the message " Windows could not finf the sw for your device" 

I tried even with mmwave_dfp_00_07_00_04 package same results.

BR,

Fabrizio