Part Number: TDC1000-TDC7200EVM
Hello,
I am working on flow measurement for water. There are certain issues Im facing. I have Steminic transducers (ones given as samples) and some samples from alibaba for flow measurement.The confiuration is that I am just keeping these transudcers in air and moving them so that I can detect signals.
1. In Mode 0 both these transducers are working but what I have noticed is for the same configuration at COMPIN the alibaba transducer has lower peaks.
2.In Mode 1 and 2 (which require 2 transducers to work with), I can detect signals if both transducers are Steminic but not with my transducers.
3. In Mode 1 and 2 if I remove one of the Steminic transducer then also the TOF measurements goes on. Dies it go back to Mode 0 if 2 transducers are not detected.
4. As soon I replace with my transducer in Mode 1 and 2 the TOF measurement stops and as i replace with Steminic it starts.
5. How do I choose transducers. I have read somewhere that the sample transducers are not good for flow measurement . Why so? Whats makes a transducer a good transducer to work with?
Regards,
Prudhvi Sagar
xinhaitai.en.alibaba.com/.../1_mhz_ultrasonic_transducer_waterproof_manufacturer_in_China.html