Other Parts Discussed in Thread: AWR1243
All,
LP87524 outputs 3.3V, 1.2V, 1.8V, and 2.3V on AWR1243 EVM board. I guess it is the default setting of the LP87524 since I disconnect the I2C from the LP87524, the chip still works fine.
What should I need to do if I want to change the output to 3.3V, 1.2V, 1.3V, and 2.1V instead of the default setting values? I need to use these new voltage in my new awr1243 design.
Do I need to program it through I2C to change the voltage?
Please help me solve this issue
Thanks a lot!