I am troubleshooting someone else's design. The output has steps of +1.5C or -1.5C. Additionally, temperature is reported at 10-15C below expectation. When the 1.5C steps are added into the data, as if to "correct" the data, I see that the reported rate of increase is the same, before and after the jumps.
Wiring: Address 0x4F; operating at 3.3V; SDA & SCL are connected to micro-controller via two 33R resistors, no pull ups to 3.3V; Alert is not connect nor pulled up.