This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642: mmw_dss build error?

Part Number: AWR1642
Other Parts Discussed in Thread: SYSBIOS, MATHLIB

hello,

when i import mmw_dss project into ccs.then  rebuild,the console display as below.

I want to configure this error and warning whether affect outputing of the xwr16xx_mmw_dss.xe674 file and .xwr16xx_mmw_dss.bin.

**** Build of configuration Debug for project mmw_dss ****

"C:\\ti\\ccsv7\\utils\\bin\\gmake" -k -j 8 all -O
rm -f F:/CCS_Programs/workspace_v7/mmw_dss/xwr16xx_mmw_dss.bin
makefile:188: recipe for target 'pre-build' failed
process_begin: CreateProcess(NULL, rm -f F:/CCS_Programs/workspace_v7/mmw_dss/xwr16xx_mmw_dss.bin, ...) failed.
make (e=2): 系统找不到指定的文件。

gmake[1]: [pre-build] Error 2 (ignored)
' '
'Building file: ../dss_mmw.cfg'
'Invoking: XDCtools'
"C:/ti/xdctools_3_50_01_12_core/xs" --xdcpath="C:/ti/bios_6_50_01_12/packages;C:/ti/ccsv7/ccs_base;" xdc.tools.configuro -o configPkg -t ti.targets.elf.C674 -p ti.platforms.c6x:IWR16XX:false:600 -r release -c "C:/ti/ccsv7/tools/compiler/ti-cgt-c6000_8.1.3" "../dss_mmw.cfg"
making package.mak (because of package.bld) ...
generating interfaces for package configPkg (because package/package.xdc.inc is older than package.xdc) ...
configuring dss_mmw.xe674 from package/cfg/dss_mmw_pe674.cfg ...
generating custom ti.sysbios library makefile ...
Starting build of library sources ...
making F:/CCS_Programs/workspace_v7/mmw_dss/src/sysbios/sysbios.ae674 ...
gmake[1]: Entering directory `F:/CCS_Programs/workspace_v7/mmw_dss/src/sysbios'
cle674 C:/ti/bios_6_50_01_12/packages/ti/sysbios/BIOS.c ...
asme674 C:/ti/bios_6_50_01_12/packages/ti/sysbios/family/c64p/Exception_asm.s64P ...
asme674 C:/ti/bios_6_50_01_12/packages/ti/sysbios/family/c64p/Hwi_asm.s62 ...
asme674 C:/ti/bios_6_50_01_12/packages/ti/sysbios/family/c64p/Hwi_asm_switch.s62 ...
asme674 C:/ti/bios_6_50_01_12/packages/ti/sysbios/family/c64p/Hwi_disp_always.s64P ...
asme674 C:/ti/bios_6_50_01_12/packages/ti/sysbios/rts/ti/tls_get_tp.asm ...
asme674 C:/ti/bios_6_50_01_12/packages/ti/sysbios/family/c62/TaskSupport_asm.s62 ...
are674 BIOS.obj c64p_Exception_asm.obj c64p_Hwi_asm.obj c64p_Hwi_asm_switch.obj c64p_Hwi_disp_always.obj ti_tls_get_tp.obj c62_TaskSupport_asm.obj ...
gmake[1]: Leaving directory `F:/CCS_Programs/workspace_v7/mmw_dss/src/sysbios'
Build of libraries done.
cle674 package/cfg/dss_mmw_pe674.c ...
"C:/ti/bios_6_50_01_12/packages/ti/sysbios/knl/Task.c", line 819: remark #270-D: declaration may not appear after executable statement in block
"C:/ti/bios_6_50_01_12/packages/ti/sysbios/timers/rti/Timer.c", line 92: remark #2142-D: comparison between signed and unsigned operands
"C:/ti/bios_6_50_01_12/packages/ti/sysbios/timers/rti/Timer.c", line 187: remark #2142-D: comparison between signed and unsigned operands
'Finished building: ../dss_mmw.cfg'
' '
'Building file: ../dss_config_edma_util.c'
'Invoking: C6000 Compiler'
"C:/ti/ccsv7/tools/compiler/ti-cgt-c6000_8.1.3/bin/cl6x" -mv6740 --abi=eabi -O3 --include_path="F:/CCS_Programs/workspace_v7/mmw_dss" --include_path="C:/ti/mmwave_sdk_01_00_00_05/packages" --include_path="C:/ti/mathlib_c674x_3_1_2_1/packages" --include_path="C:/ti/dsplib_c64Px_3_4_0_0/packages/ti/dsplib/src/DSP_fft16x16/c64P" --include_path="C:/ti/dsplib_c64Px_3_4_0_0/packages/ti/dsplib/src/DSP_fft32x32/c64P" --include_path="C:/ti/ccsv7/tools/compiler/ti-cgt-c6000_8.1.3/include" -g --gcc --define=SOC_XWR16XX --define=SUBSYS_DSS --define=DOWNLOAD_FROM_CCS --define=DebugP_ASSERT_ENABLED --diag_wrap=off --diag_warning=225 --display_error_number --gen_func_subsections=on --obj_extension=.oe674 --preproc_with_compile --preproc_dependency="dss_config_edma_util.d" --cmd_file="configPkg/compiler.opt" "../dss_config_edma_util.c"
'Finished building: ../dss_config_edma_util.c'
' '
'Building file: ../gen_twiddle_fft32x32.c'
'Invoking: C6000 Compiler'
"C:/ti/ccsv7/tools/compiler/ti-cgt-c6000_8.1.3/bin/cl6x" -mv6740 --abi=eabi -O3 --include_path="F:/CCS_Programs/workspace_v7/mmw_dss" --include_path="C:/ti/mmwave_sdk_01_00_00_05/packages" --include_path="C:/ti/mathlib_c674x_3_1_2_1/packages" --include_path="C:/ti/dsplib_c64Px_3_4_0_0/packages/ti/dsplib/src/DSP_fft16x16/c64P" --include_path="C:/ti/dsplib_c64Px_3_4_0_0/packages/ti/dsplib/src/DSP_fft32x32/c64P" --include_path="C:/ti/ccsv7/tools/compiler/ti-cgt-c6000_8.1.3/include" -g --gcc --define=SOC_XWR16XX --define=SUBSYS_DSS --define=DOWNLOAD_FROM_CCS --define=DebugP_ASSERT_ENABLED --diag_wrap=off --diag_warning=225 --display_error_number --gen_func_subsections=on --obj_extension=.oe674 --preproc_with_compile --preproc_dependency="gen_twiddle_fft32x32.d" --cmd_file="configPkg/compiler.opt" "../gen_twiddle_fft32x32.c"
'Finished building: ../gen_twiddle_fft32x32.c'
' '
'Building file: ../gen_twiddle_fft16x16.c'
'Invoking: C6000 Compiler'
"C:/ti/ccsv7/tools/compiler/ti-cgt-c6000_8.1.3/bin/cl6x" -mv6740 --abi=eabi -O3 --include_path="F:/CCS_Programs/workspace_v7/mmw_dss" --include_path="C:/ti/mmwave_sdk_01_00_00_05/packages" --include_path="C:/ti/mathlib_c674x_3_1_2_1/packages" --include_path="C:/ti/dsplib_c64Px_3_4_0_0/packages/ti/dsplib/src/DSP_fft16x16/c64P" --include_path="C:/ti/dsplib_c64Px_3_4_0_0/packages/ti/dsplib/src/DSP_fft32x32/c64P" --include_path="C:/ti/ccsv7/tools/compiler/ti-cgt-c6000_8.1.3/include" -g --gcc --define=SOC_XWR16XX --define=SUBSYS_DSS --define=DOWNLOAD_FROM_CCS --define=DebugP_ASSERT_ENABLED --diag_wrap=off --diag_warning=225 --display_error_number --gen_func_subsections=on --obj_extension=.oe674 --preproc_with_compile --preproc_dependency="gen_twiddle_fft16x16.d" --cmd_file="configPkg/compiler.opt" "../gen_twiddle_fft16x16.c"
'Finished building: ../gen_twiddle_fft16x16.c'
' '
'Building file: ../dss_main.c'
'Invoking: C6000 Compiler'
"C:/ti/ccsv7/tools/compiler/ti-cgt-c6000_8.1.3/bin/cl6x" -mv6740 --abi=eabi -O3 --include_path="F:/CCS_Programs/workspace_v7/mmw_dss" --include_path="C:/ti/mmwave_sdk_01_00_00_05/packages" --include_path="C:/ti/mathlib_c674x_3_1_2_1/packages" --include_path="C:/ti/dsplib_c64Px_3_4_0_0/packages/ti/dsplib/src/DSP_fft16x16/c64P" --include_path="C:/ti/dsplib_c64Px_3_4_0_0/packages/ti/dsplib/src/DSP_fft32x32/c64P" --include_path="C:/ti/ccsv7/tools/compiler/ti-cgt-c6000_8.1.3/include" -g --gcc --define=SOC_XWR16XX --define=SUBSYS_DSS --define=DOWNLOAD_FROM_CCS --define=DebugP_ASSERT_ENABLED --diag_wrap=off --diag_warning=225 --display_error_number --gen_func_subsections=on --obj_extension=.oe674 --preproc_with_compile --preproc_dependency="dss_main.d" --cmd_file="configPkg/compiler.opt" "../dss_main.c"
"C:/ti/mathlib_c674x_3_1_2_1/packages/ti/mathlib/src/common/common.h", line 55: warning #48-D: incompatible redefinition of macro "TRUE" (declared at line 322 of "C:/ti/xdctools_3_50_01_12_core/packages/xdc/std.h")
"C:/ti/mathlib_c674x_3_1_2_1/packages/ti/mathlib/src/common/common.h", line 56: warning #48-D: incompatible redefinition of macro "FALSE" (declared at line 319 of "C:/ti/xdctools_3_50_01_12_core/packages/xdc/std.h")
'Finished building: ../dss_main.c'
' '
'Building file: ../dss_data_path.c'
'Invoking: C6000 Compiler'
"C:/ti/ccsv7/tools/compiler/ti-cgt-c6000_8.1.3/bin/cl6x" -mv6740 --abi=eabi -O3 --include_path="F:/CCS_Programs/workspace_v7/mmw_dss" --include_path="C:/ti/mmwave_sdk_01_00_00_05/packages" --include_path="C:/ti/mathlib_c674x_3_1_2_1/packages" --include_path="C:/ti/dsplib_c64Px_3_4_0_0/packages/ti/dsplib/src/DSP_fft16x16/c64P" --include_path="C:/ti/dsplib_c64Px_3_4_0_0/packages/ti/dsplib/src/DSP_fft32x32/c64P" --include_path="C:/ti/ccsv7/tools/compiler/ti-cgt-c6000_8.1.3/include" -g --gcc --define=SOC_XWR16XX --define=SUBSYS_DSS --define=DOWNLOAD_FROM_CCS --define=DebugP_ASSERT_ENABLED --diag_wrap=off --diag_warning=225 --display_error_number --gen_func_subsections=on --obj_extension=.oe674 --preproc_with_compile --preproc_dependency="dss_data_path.d" --cmd_file="configPkg/compiler.opt" "../dss_data_path.c"
"C:/ti/mathlib_c674x_3_1_2_1/packages/ti/mathlib/src/common/common.h", line 55: warning #48-D: incompatible redefinition of macro "TRUE" (declared at line 322 of "C:/ti/xdctools_3_50_01_12_core/packages/xdc/std.h")
"C:/ti/mathlib_c674x_3_1_2_1/packages/ti/mathlib/src/common/common.h", line 56: warning #48-D: incompatible redefinition of macro "FALSE" (declared at line 319 of "C:/ti/xdctools_3_50_01_12_core/packages/xdc/std.h")
'Finished building: ../dss_data_path.c'
' '
'Building target: xwr16xx_mmw_dss.xe674'
'Invoking: C6000 Linker'
"C:/ti/ccsv7/tools/compiler/ti-cgt-c6000_8.1.3/bin/cl6x" -mv6740 --abi=eabi -O3 -g --gcc --define=SOC_XWR16XX --define=SUBSYS_DSS --define=DOWNLOAD_FROM_CCS --define=DebugP_ASSERT_ENABLED --diag_wrap=off --diag_warning=225 --display_error_number --gen_func_subsections=on --obj_extension=.oe674 -z -m"xwr16xx_mmw_dss.map" --stack_size=0x800 --heap_size=0x800 -i"C:/ti/mmwave_sdk_01_00_00_05/packages/ti/control/mmwave/lib" -i"C:/ti/mmwave_sdk_01_00_00_05/packages/ti/control/mmwavelink/lib" -i"C:/ti/mmwave_sdk_01_00_00_05/packages/ti/drivers/crc/lib" -i"C:/ti/mmwave_sdk_01_00_00_05/packages/ti/drivers/mailbox/lib" -i"C:/ti/mmwave_sdk_01_00_00_05/packages/ti/drivers/osal/lib" -i"C:/ti/mmwave_sdk_01_00_00_05/packages/ti/drivers/soc/lib" -i"C:/ti/mmwave_sdk_01_00_00_05/packages/ti/drivers/uart/lib" -i"C:/ti/mmwave_sdk_01_00_00_05/packages/ti/drivers/edma/lib" -i"C:/ti/mmwave_sdk_01_00_00_05/packages/ti/drivers/adcbuf/lib" -i"C:/ti/mmwave_sdk_01_00_00_05/packages/ti/alg/mmwavelib/lib" -i"C:/ti/dsplib_c64Px_3_4_0_0/packages/ti/dsplib/lib" -i"C:/ti/mathlib_c674x_3_1_2_1/packages/ti/mathlib/lib" -i"C:/ti/ccsv7/tools/compiler/ti-cgt-c6000_8.1.3/lib" -i"C:/ti/ccsv7/tools/compiler/ti-cgt-c6000_8.1.3/include" --reread_libs --disable_auto_rts --diag_warning=225 --diag_wrap=off --warn_sections --display_error_number --xml_link_info="xwr16xx_mmw_dss_linkInfo.xml" --ram_model --unused_section_elimination=on -o "xwr16xx_mmw_dss.xe674" "./dss_config_edma_util.oe674" "./dss_data_path.oe674" "./dss_main.oe674" "./gen_twiddle_fft16x16.oe674" "./gen_twiddle_fft32x32.oe674" "../c674x_linker.cmd" "../dss_mmw_linker.cmd" -l"configPkg/linker.cmd" -llibosal_xwr16xx.ae674 -llibsoc_xwr16xx.ae674 -llibcrc_xwr16xx.ae674 -llibuart_xwr16xx.ae674 -llibmailbox_xwr16xx.ae674 -llibmmwavelink_xwr16xx.ae674 -llibmmwave_xwr16xx.ae674 -lmathlib.ae674 -ldsplib.ae64P -llibedma_xwr16xx.ae674 -llibadcbuf_xwr16xx.ae674 -llibmmwavealg_xwr16xx.ae674 -lrts6740_elf.lib -llibc.a
<Linking>
"../dss_mmw_linker.cmd", line 44: warning #10068-D: no matching section
'Finished building target: xwr16xx_mmw_dss.xe674'
' '
C:/ti/mmwave_sdk_01_00_00_05/packages/scripts/ImageCreator/xwr16xx/out2rprc/out2rprc.exe xwr16xx_mmw_dss.xe674 xwr16xx_mmw_dss.bin
Parsing the input object file, xwr16xx_mmw_dss.xe674.
Appending zeros 8463904
Appending zeros 8471568
Appending zeros 8480656
Appending zeros 8481280
File conversion complete!
' '

**** Build Finished ****

  • The first several lines show that errors occur during build. This is the path difference: ccs7 folder was assumed to be in C disk but asked to search under F disk.

    After that, it seems build was running fine. Generating xe674 file in the end. There is warning but no errors. If the question is only a concern over the warning message, I suggest ignore it and go ahead with the mss build and then demo.

    If there's issue with build, please let me know the tirex version you downloaded. Thanks!

    Regards,
    Michelle
  • hello,
    I have already resolved my question.I just ignore it.Thanks