This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642BOOST: AWR1642 Booster Pack - Out of box demo : Not able to receive detected objects data in RS232 Tx and Rx Connector pins in J6

Part Number: AWR1642BOOST
Other Parts Discussed in Thread: AWR1642

We are trying to interface AWR1642 Booster pack to CC3220 Launchpad to receive detected objects via Uart.  We run out of the box demo in mmwave sdk and tried connected Pin5 and 7 in Booster pack to Pin 3 and 4 of cc3220 Launchpad . But we are not able to receive any data in uart pins.

Could you please help us to send the detected objects through uart Pins 5 and 7 ? What changes should we do in Uart driver to transmit the data through connector uart pins ?

  • Hello Sneha,
    The mmw demo application sends the object data on pin F14 of the AWR1642 device (net name of the signal is AR_MSS_LOGGER). It uses the RS232 RX and TX port (pin 3 and 4 of the Booster pack connector) to send the configuration from PC to the AWR device. If you want to change this setting you can change the code with different pin up option.

    Regards,
    Vivek