Other Parts Discussed in Thread: PGA460, USB2ANY
Hello,
I need to perform deeper tests with the PGA460. For that purpose, I would need :
1) to program the device
2) to display the echo dump visually
3) to have a sub-milimetric display of the distance that I could log in a file
For 1) and 2), the GUI is really perfect. My only issue is for 3) : currently, the GUI displays meters in the form x.xxx m. I would need one more digit for my tests. I can trigger the Burst/Listen command and then read the Measurements Results from the Interface tab, but I cannot do it in loop nor save the results in a file.
I could basically also write a small script by myself which would perform 3), but as the USB2ANY protocol is closed, I don't know what bytes to send.
Could you help me on the topic ?
Thanks,
Sam