This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/AWR1642: awr1642

Part Number: AWR1642


Tool/software: Code Composer Studio

What is the minimal output power detectable from the rx antenna??

  • Hello Christian,
    By the term "detectable" do you mean the detectable as a actual object in the radar processing ? That would depend on the detection algorithm used by you, the SNR thresholds for the detection etc. From the RX analog/RF chain perspective there is only a noise figure number suggested in the datasheet , which is typically 15dB in the 76-77 Ghz band.

    Regards,
    Vivek
  • thank you for the request. i got it!

    Mit freundlichen Grüßen / Best regards /Meilleures Salutations

    Herr Christian joel Mougang Nganmenie
    Bachelorand
    Valeo Comfort & Driving Assistance (CDA)
    Valeo Radar Systems (DAS-E-RAD)

    Site Bietigheim
    Tel:  +4971429163729      
    E-Mail:  Christian-Joel.Mougang-Nganmenie@valeo.com

    Location:
    Active Safety Center (ASC)
    Stuttgarter Strasse 75 
    74321 Bietigheim-Bissingen

    Postal Adress:
    Valeo Schalter und Sensoren GmbH
    Laiernstrasse 12
    74321 Bietigheim-Bissingen


    Valeo Schalter und Sensoren GmbH
    Laiernstrasse 12
    74321 Bietigheim-Bissingen, 
    Sitz der Gesellschaft: 74321 Bietigheim-Bissingen
    Handelsregister: Amtsgericht Stuttgart - HRB 301795
    Vorsitzender des Aufsichtsrates: Derrick Zechmair
    Geschäftsführer: Jens Hälker, Martin Mandry, Stiv Michael Smudja, Pierre-Yves Veltois