Hello,
I'm trying to flash CCS debug firmware. I need to power cycle the device before I load images. Is there a button to power cycle the device on the EVM or I just simply remove the power and power up the EVM again?
In addition, is the attached file ADC Data Capture SDK1.05 V1.00.pdf outdated because the latest SDK version is 1.1.0.2 or I can still follow the steps in this file?4353.ADC Data Capture SDK1.05 V1.00.pdf
Thanks,
Yun