Other Parts Discussed in Thread: AWR1642, IWR1642
Tool/software: Code Composer Studio
Hello,
When I load demo programs onto an AWR1642 using CCS, the program runs fine during configuration before sending a sensorStart event. However, upon receiving a sensorStart event, the Cortex R4 disconnects in CCS. The error log for it is below:
IcePick_M_0: Error: (Error -261 @ 0xFFFFFEFB) Invalid response was received from the XDS110. (Emulation package 7.0.48.0)
CS_DAP_0: Error: (Error -261 @ 0x0) Invalid response was received from the XDS110. (Emulation package 7.0.48.0)
Cortex_R4_0: Error: (Error -261 @ 0x0) Invalid response was received from the XDS110. (Emulation package 7.0.48.0)
CS_DAP_0: Unable to determine target status after 20 attempts
CS_DAP_0: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
Cortex_R4_0: Unable to determine target status after 20 attempts
Cortex_R4_0: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
I've tested with multiple different radars, and the same issue occurs with each of them.
Any help is much appreciated!
[unlocked 1/24/18]>LE