This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1243: Data rate for CSI2/LVDS

Part Number: AWR1243


Hi, 

From the AWR1243 product sheet (page 30):

CSI-2 data rate scalable from 150 Mbps to 900 Mbps per lane (If four lanes are used simultaneously then the maximum data rate supported is 600 Mbps per lane). 

My question is why does the data rate get limited to 600 Mbps per lane if all channels are being used ?

Will the data rate increase in production samples or will it be capped at 600 Mbps if 4 lanes are ON ?

Regards,

RJ